S32K116 JTAG Program error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K116 JTAG Program error

3,325 次查看
rjmalmeida0
Contributor III

Hi,
I'm currently using the S32K116 microcontroller. When I flashed a previously working program using JTAG into the microcontroller, it asserted an error during flashing/debugging and the microcontroller entered into the DefaultISR handler. When I flashed I got this error: ERROR: Could not detect CPU clock speed. Failed to execute RAMcode for RAM check.

Any ideas how to fix this issue?

Regards,

Rui Almeida

标签 (1)
0 项奖励
回复
3 回复数

3,239 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

What programmer / IDE are you using?

Can you re-flash the MCU with another project/example?

If so, can you share the project that cannot be loaded?

Thanks,

BR, Daniel

0 项奖励
回复

3,239 次查看
rjmalmeida0
Contributor III

Hello Daniel,

I'm using the S32 Design Studio and Segger JLINK debugger. When I flashed the MCU with another project, it goes straight to Reset handler without even entering SystemInit or main function.

0 项奖励
回复

3,239 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Rui,

Since this is a Segger error message, I would recommend contacting their support:

J-Link/Flasher related - SEGGER - Forum 

If you have an EVB, have you tried reprogramming it with OpenSDA?

Or do you have any other programmer?

BR, Daniel

0 项奖励
回复