S32K116 Firmware Upgrade

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116 Firmware Upgrade

1,622 Views
geokpeng_tan
Contributor I

Hi, I am currently looking at S32K116 series MCU, would like to know the firmware upgrade via UART.

So for the UART, do I need to connect two lines (Rx,Tx) only or 4 lines with flow control?

0 Kudos
Reply
1 Reply

1,540 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to recommend you AN12218 S32K1xx Serial Bootloader with SW located on this link in the Application note section 32-bit Automotive General Purpose MCUs | NXP 

Hardware flow control is supported but it depends on your application requirements. You do not have to use it. 

I hope it helps.

Best Regards,

Diana

0 Kudos
Reply