S32K116 Firmware Upgrade

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 Firmware Upgrade

1,615件の閲覧回数
geokpeng_tan
Contributor I

Hi, I am currently looking at S32K116 series MCU, would like to know the firmware upgrade via UART.

So for the UART, do I need to connect two lines (Rx,Tx) only or 4 lines with flow control?

0 件の賞賛
返信
1 返信

1,533件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I would like to recommend you AN12218 S32K1xx Serial Bootloader with SW located on this link in the Application note section 32-bit Automotive General Purpose MCUs | NXP 

Hardware flow control is supported but it depends on your application requirements. You do not have to use it. 

I hope it helps.

Best Regards,

Diana

0 件の賞賛
返信