S32K116 CAN FD Support status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 CAN FD Support status

ソリューションへジャンプ
4,309件の閲覧回数
Oido
Contributor III

Does S32K116 support 2Mbps CAN FD with FIRC?

CAN 1x with 116 and 118 models tied to the data sheet
It says (1x with FD), but CHAT GPT informed that S32K116 does not support CAN FD, but from S32K118 onwards model, CAN FD is supported.
I'd like to know a clear answer.

0 件の賞賛
返信
1 解決策
4,211件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,282件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

No, for S32K116LIV,it does't support CAN FD

Senlent_0-1747794977412.png

 

0 件の賞賛
返信
4,258件の閲覧回数
Oido
Contributor III

Thank you for your answer.
FS32K116LAT0MLFR If I use this model, will I be able to use both CAN-FD and PWM?

0 件の賞賛
返信
4,246件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

There is noting to do with PWM, PWM can be generated from FTM module.

FlexIo module can also used to generate PWM.

0 件の賞賛
返信
4,233件の閲覧回数
Oido
Contributor III

In conclusion, by replacing FS32K116LAT0MLFR with model, is it correct that I can use PWM with Flexio function and CAN-FD (2M 64byte) instead of classic-CAN (500K 8byte)? I haven't heard back about CAN-FD yet.

0 件の賞賛
返信
4,212件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

0 件の賞賛
返信
4,300件の閲覧回数
Oido
Contributor III

In my MCU, the letters are written like S32K116LIV.

0 件の賞賛
返信