S32K116 CAN FD Support status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116 CAN FD Support status

Jump to solution
4,311 Views
Oido
Contributor III

Does S32K116 support 2Mbps CAN FD with FIRC?

CAN 1x with 116 and 118 models tied to the data sheet
It says (1x with FD), but CHAT GPT informed that S32K116 does not support CAN FD, but from S32K118 onwards model, CAN FD is supported.
I'd like to know a clear answer.

0 Kudos
Reply
1 Solution
4,213 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

View solution in original post

0 Kudos
Reply
6 Replies
4,284 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

No, for S32K116LIV,it does't support CAN FD

Senlent_0-1747794977412.png

 

0 Kudos
Reply
4,260 Views
Oido
Contributor III

Thank you for your answer.
FS32K116LAT0MLFR If I use this model, will I be able to use both CAN-FD and PWM?

0 Kudos
Reply
4,248 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

There is noting to do with PWM, PWM can be generated from FTM module.

FlexIo module can also used to generate PWM.

0 Kudos
Reply
4,235 Views
Oido
Contributor III

In conclusion, by replacing FS32K116LAT0MLFR with model, is it correct that I can use PWM with Flexio function and CAN-FD (2M 64byte) instead of classic-CAN (500K 8byte)? I haven't heard back about CAN-FD yet.

0 Kudos
Reply
4,214 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

0 Kudos
Reply
4,302 Views
Oido
Contributor III

In my MCU, the letters are written like S32K116LIV.

0 Kudos
Reply