S32K116 CAN FD Support status

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K116 CAN FD Support status

跳至解决方案
4,328 次查看
Oido
Contributor III

Does S32K116 support 2Mbps CAN FD with FIRC?

CAN 1x with 116 and 118 models tied to the data sheet
It says (1x with FD), but CHAT GPT informed that S32K116 does not support CAN FD, but from S32K118 onwards model, CAN FD is supported.
I'd like to know a clear answer.

0 项奖励
回复
1 解答
4,230 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,301 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

No, for S32K116LIV,it does't support CAN FD

Senlent_0-1747794977412.png

 

0 项奖励
回复
4,277 次查看
Oido
Contributor III

Thank you for your answer.
FS32K116LAT0MLFR If I use this model, will I be able to use both CAN-FD and PWM?

0 项奖励
回复
4,265 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

There is noting to do with PWM, PWM can be generated from FTM module.

FlexIo module can also used to generate PWM.

0 项奖励
回复
4,252 次查看
Oido
Contributor III

In conclusion, by replacing FS32K116LAT0MLFR with model, is it correct that I can use PWM with Flexio function and CAN-FD (2M 64byte) instead of classic-CAN (500K 8byte)? I haven't heard back about CAN-FD yet.

0 项奖励
回复
4,231 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oido

yes, this part number can support FLEXIO and CAN FD.

0 项奖励
回复
4,319 次查看
Oido
Contributor III

In my MCU, the letters are written like S32K116LIV.

0 项奖励
回复