S32K1 ADC channel naming convention

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 ADC channel naming convention

Jump to solution
1,731 Views
Jimny
Contributor II

hello,

I am confused with the ADC channel naming.

In S32DS processor expert, the channel naming scheme is shown in the picture below.

1.PNG

But in the reference manual, it uses ADC0_SE0, ADC0_SE1, ..., to name the adc channels.

How can I relate the two naming schemes? E.g., does ADC_INPUTCHAN_EXT0 relate to ADC0_SE0? And what about ADC1_SE0?

0 Kudos
Reply
1 Solution
1,723 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the confusion.
ADC_INPUTCHAN_EXT0 relate to ADCx_SE0

Device Input Channel.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
1 Reply
1,724 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the confusion.
ADC_INPUTCHAN_EXT0 relate to ADCx_SE0

Device Input Channel.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply