S32K mass program tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K mass program tools

Jump to solution
5,246 Views
hansonhe
NXP Employee
NXP Employee

Dear,

As we known, we could use IAR or S32DS for S32K debug and download, whether we have some offline GUI or USB standalone tools for firmware downloading, it is only program update without debug, such as Segger company J-Flash software for cortex M0, M3, M4.

0 Kudos
Reply
1 Solution
4,617 Views
hansonhe
NXP Employee
NXP Employee

Dear, we have closed by ourselves, now Segger could support S32K144.

View solution in original post

0 Kudos
Reply
4 Replies
4,617 Views
songhanson
Contributor I

Hi Hanson,

可以使用Segger的Flasher,目前JFlash已经支持S32K的下载,JFlash配置好目标芯片S32K后,然后选择download到Flasher中,然后按下按键即可对目标芯片离线烧写。

1.png

或者参考我的iFlasher:

MiniFlasherS.jpg

具体描述:

MiniFlasher | Thanks For Everything. 

0 Kudos
Reply
4,617 Views
Daniel_Popa
NXP Employee
NXP Employee

Is this How To Program the Application in the Flash/RAM what you are looking for ?

The program is called RAppID_BL and is available here

Best regards,
Daniel

0 Kudos
Reply
4,617 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify your question? From your post I am not sure what are you asking for.

Regards,

Martin

0 Kudos
Reply
4,618 Views
hansonhe
NXP Employee
NXP Employee

Dear, we have closed by ourselves, now Segger could support S32K144.

0 Kudos
Reply