S32K lpuart receive dynamic byte sizes at once with interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K lpuart receive dynamic byte sizes at once with interrupt

1,995 次查看
afa25
Contributor II

Hi,

I am trying to get uart messages with interrupt. I have seen examples with interrupts however, these examples take the message one byte at a time. I wonder if there is a way to get whole bytes at once.

For example: if I send a message to the board with size 5, ISR should get 5 bytes at once. After that, if I send 47 bytes as an example, ISR should get 47 bytes at once.

Thank you.

标记 (3)
0 项奖励
回复
4 回复数

1,977 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @afa25 

In the UART chapter of the S32K1 and S32K3 reference manuals, you can find that most family variants have a FIFO that supports 4 words, and some instances support 16.
In other words, the maximum number of characters you could receive per interrupt is the total size of the FIFO.
I can suggest using the UART with DMA together to handle a more significant amount of data.

 

B.R.

VaneB

0 项奖励
回复

1,969 次查看
afa25
Contributor II
Thank you,

Is there any simple example project related to LpUart with DMA?
0 项奖励
回复

1,965 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @afa25 

Unfortunately, we do not have LPUART DMA examples or training material.

However, there is a LpuartFlexio_Uart_Ip_Example RTD example that can be modified.

  1. Change the Uart method from Using Interrupts to Using DMA in the GUI of the UART driver.
  2. Add DMA driver to the project (Dma_Ip)
  3. Add DMA channels in the GUI of the DMA driver (Dma logic channels)
  4. Link the DMA channels in the UART driver.
  5. Update/generate the RTD code.
  6. Initialize the DMA driver in the code (Dma_Ip_Init()).
0 项奖励
回复

1,935 次查看
afa25
Contributor II

Thank you! 

I will try it. 

0 项奖励
回复