S32K gPTP stack RTD Compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K gPTP stack RTD Compatibility

1,436件の閲覧回数
oliver777777
Contributor II

Hi, 

I'm looking to enable gPTP stack on S32Kxx based boards but noticed that the NXP provided gPTP 0.9.0 is only compatible with RTD 4.0.0, but our current system is on RTD 5.0.0. Is there any updated version of the stack.

If not, how would you advise me to proceed to enable gPTP on our current system? I see the MAC_Timestamp_Control register as well as section 75.8 in the RM. Are there any other registers/sections of interest I should look at? 

Thanks

 

 

0 件の賞賛
返信
1 返信

1,391件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hi @oliver777777 ,

Unfortunately, it is recommended to use gPTP 0.9.0 with RTD 4.0.0.

MAC_Timestamp_Control is the key one.

Best regards,

Pavel

0 件の賞賛
返信