S32K_PN Compatibility Issue_FC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K_PN Compatibility Issue_FC

跳至解决方案
2,897 次查看
Fidel
Contributor IV

Dears,

        Actually, I need S32KNHT1MPBST for my project, but now I only have S32KEHT1MPBST on hand, so here I want to know if they have hardware level diff between of them? or the difference is only about the IPs in them, and I can replace S32KNHT1MPBST with S32KEHT1MPBST  completley? 

       thanks a lot~

0 项奖励
回复
1 解答
2,866 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 项奖励
回复
6 回复数
2,883 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, could you please double check mentioned part numbers? I don't think these are existing devices. Are they supposed to be MCUs or some boards / other equipment? Please clarify

0 项奖励
回复
2,880 次查看
Fidel
Contributor IV

Hi, Sorry, I forgot the "344", it  should be S32K344NHT1MPBST  and S32K344EHT1MPBST.

0 项奖励
回复
2,871 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

The only difference is missing Ethernet, in other aspect both derivatives are equal.

0 项奖励
回复
2,869 次查看
Fidel
Contributor IV

That means both can be used to replace each other pin 2 pin on hardware level if Ethernet was not used, that is right?

0 项奖励
回复
2,867 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is.

0 项奖励
回复
2,864 次查看
Fidel
Contributor IV

got it ,thanks a lot~

0 项奖励
回复