S32K OTA Rollback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K OTA Rollback

Jump to solution
394 Views
RootOf3
Contributor II

各位好,我想咨询一下,关于S32K3系列的HSE ABSwap OTA回滚机制。我了解到的是如果A区为稳定区,将A区切换到B区,B区如果出现Hardfault或看门狗超时等错误问题,OTA的错误计数器会累减,当错误计数器为0时,程序会认定B区为不稳定区从而切换片区回到A区。请问这个机制是正确的吗?如果不是,那么OTA的回滚机制是怎样的呢?

0 Kudos
Reply
1 Solution
355 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @RootOf3 

 

For S32K3 HSE AB Swap, the rollback mechanism is not based on HSE monitoring runtime failures such as HardFaults or watchdog resets.

 

HSE itself does not determine whether the newly activated application is stable based on the application runtime behavior. After the AB Swap is performed, the new image becomes active, and it is typically the responsibility of the user bootloader/application to decide whether the update was successful or whether a rollback should be requested.

 

Secure Boot can also be used as part of the recovery strategy. If authentication of the active image fails, the boot flow can be designed to execute an alternate image or a dedicated recovery image, depending on the configured boot flow and the customer’s software design. Once a valid recovery or alternate image is running, the software can request another AB Swap if needed.

 

So, in summary, HSE provides the mechanisms for Secure Boot, image authentication, and AB Swap, but the actual rollback policy, including how runtime failures are detected and when the system switches back to the previous image, is implemented by the user bootloader/application.

 

Regards,

Lukas

View solution in original post

1 Reply
356 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @RootOf3 

 

For S32K3 HSE AB Swap, the rollback mechanism is not based on HSE monitoring runtime failures such as HardFaults or watchdog resets.

 

HSE itself does not determine whether the newly activated application is stable based on the application runtime behavior. After the AB Swap is performed, the new image becomes active, and it is typically the responsibility of the user bootloader/application to decide whether the update was successful or whether a rollback should be requested.

 

Secure Boot can also be used as part of the recovery strategy. If authentication of the active image fails, the boot flow can be designed to execute an alternate image or a dedicated recovery image, depending on the configured boot flow and the customer’s software design. Once a valid recovery or alternate image is running, the software can request another AB Swap if needed.

 

So, in summary, HSE provides the mechanisms for Secure Boot, image authentication, and AB Swap, but the actual rollback policy, including how runtime failures are detected and when the system switches back to the previous image, is implemented by the user bootloader/application.

 

Regards,

Lukas

%3CLINGO-SUB%20id%3D%22lingo-sub-2399857%22%20slang%3D%22zh-CN%22%20mode%3D%22CREATE%22%3ES32K%20OTA%20Rollback%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2399857%22%20slang%3D%22zh-CN%22%20mode%3D%22CREATE%22%3E%3CP%3EHello%20everyone%2C%20I'd%20like%20to%20inquire%20about%20the%20HSE%20ABSwap%20OTA%20rollback%20mechanism%20for%20the%20S32K3%20series.%20My%20understanding%20is%20that%20if%20partition%20A%20is%20a%20stable%20partition%2C%20switching%20from%20partition%20A%20to%20partition%20B%20will%20cause%20errors%20such%20as%20Hardfault%20or%20watchdog%20timeout%20to%20occur%20in%20partition%20B.%20The%20OTA%20error%20counter%20will%20decrease%2C%20and%20when%20the%20error%20counter%20reaches%200%2C%20the%20program%20will%20consider%20partition%20B%20an%20unstable%20partition%20and%20switch%20back%20to%20partition%20A.%20Is%20this%20mechanism%20correct%3F%20If%20not%2C%20what%20is%20the%20OTA%20rollback%20mechanism%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2400332%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20S32K%20OTA%20Rollback%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2400332%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F265121%22%20target%3D%22_blank%22%3E%40RootOf3%3C%2FA%3E%26nbsp%3B%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EFor%20S32K3%20HSE%20AB%20Swap%2C%20the%20rollback%20mechanism%20is%20not%20based%20on%20HSE%20monitoring%20runtime%20failures%20such%20as%20HardFaults%20or%20watchdog%20resets.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3EHSE%20itself%20does%20not%20determine%20whether%20the%20newly%20activated%20application%20is%20stable%20based%20on%20the%20application%20runtime%20behavior.%20After%20the%20AB%20Swap%20is%20performed%2C%20the%20new%20image%20becomes%20active%2C%20and%20it%20is%20typically%20the%20responsibility%20of%20the%20user%20bootloader%2Fapplication%20to%20decide%20whether%20the%20update%20was%20successful%20or%20whether%20a%20rollback%20should%20be%20requested.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3ESecure%20Boot%20can%20also%20be%20used%20as%20part%20of%20the%20recovery%20strategy.%20If%20authentication%20of%20the%20active%20image%20fails%2C%20the%20boot%20flow%20can%20be%20designed%20to%20execute%20an%20alternate%20image%20or%20a%20dedicated%20recovery%20image%2C%20depending%20on%20the%20configured%20boot%20flow%20and%20the%20customer%E2%80%99s%20software%20design.%20Once%20a%20valid%20recovery%20or%20alternate%20image%20is%20running%2C%20the%20software%20can%20request%20another%20AB%20Swap%20if%20needed.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3ESo%2C%20in%20summary%2C%20HSE%20provides%20the%20mechanisms%20for%20Secure%20Boot%2C%20image%20authentication%2C%20and%20AB%20Swap%2C%20but%20the%20actual%20rollback%20policy%2C%20including%20how%20runtime%20failures%20are%20detected%20and%20when%20the%20system%20switches%20back%20to%20the%20previous%20image%2C%20is%20implemented%20by%20the%20user%20bootloader%2Fapplication.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3ERegards%2C%3C%2FP%3E%0A%3CP%3ELukas%3C%2FP%3E%3C%2FLINGO-BODY%3E