S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

2,215件の閲覧回数
jacky_Tan
NXP Employee
NXP Employee

s32k_GPIO.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,088件の閲覧回数
jacky_Tan
NXP Employee
NXP Employee

thank you Daniel,

would you please provide that customer needs to know the voltage if the pin is loaded with 0mA? no this data in the S32K1xx datasheet.

0 件の賞賛
返信

2,088件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

The output is driven to VDD or VSS.

If the pin is not loaded, the sink/source current is 0mA, the output is equal to VDD or VSS.

Regards,

Daniel

2,088件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

What is the question here?

The specification says that the voltage drops to VDD - 0.8V when the pin is loaded with 5 mA.

Regards,

Daniel

0 件の賞賛
返信