S32K FEE Write Exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K FEE Write Exception

3,964件の閲覧回数
HuitingXu
Contributor I

Hello 

When data is written to D-flash, the allocated cluster is often not fully written, but the cluster is frequently switched. The reason is that when the remaining space of the written object sector is less than the length of the next data to be written, FEE will judge that the end address of the next write data is greater than the end address of the current sector. An error is then reported in FEE, causing the entire erase switch of the cluster to occur. How to avoid this situation?

Thanks

0 件の賞賛
返信
8 返答(返信)

3,912件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi HuitingXu,

Which version of S32K3 are you using? Because as far as I know, this issue was fixed from SW32K3_RTD_4.4_R21-11_3.0.0_P01. So, you can try to refer to it.

Best regards,

Nhi

 

タグ(1)
0 件の賞賛
返信

3,904件の閲覧回数
HuitingXu
Contributor I

Hi Nhi_Nguyen,

We are using the virsion of S32K1_RTD_4.4_1.0.1_HF01_D2209

0 件の賞賛
返信

3,890件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi HuitingXu,

For K1, please try to upgrade to the package SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_P01. I saw that your issue fixed at this version.

Best regards,

Nhi

 

0 件の賞賛
返信

3,850件の閲覧回数
HuitingXu
Contributor I

Do you have any idea about where can find the release note which include the update detail between this two version ? 

0 件の賞賛
返信

3,835件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi @HuitingXu ,

You can find the release note for each package in which you downloaded that package. For example: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=3592883 

Nhi_Nguyen_1-1695354835911.png

For your issue, this was made:

Nhi_Nguyen_0-1695354651346.png

Best regards,

Nhi

0 件の賞賛
返信

3,813件の閲覧回数
HuitingXu
Contributor I

Where can we download the package of this two versions? ( S32K1_S32M24X Real Time Drivers AUTOSAR4.4 &R21-11 version 2.0.0 / S32K1_S32M24XReal Time Drivers AUTOSAR4.4 version 2.0.0 P01)

0 件の賞賛
返信

3,818件の閲覧回数
HuitingXu
Contributor I

We need your opinion on the version replacement, which S32K1_S32M24X Real Time Drivers AUTOSAR4.4 &R21-11 version 2.0.0 or S32K1_S32M24XReal Time Drivers AUTOSAR4.4 version 2.0.0 P01 is more suitable instead of S32K1_RTD_4.4_1.0.1_HF01_D2209? Or what's the difference between this two versions? 

0 件の賞賛
返信

3,806件の閲覧回数
Nhi_Nguyen
NXP Employee
NXP Employee

Hi @HuitingXu ,

You can download at: https://are.nxp.com/FlexNetCatalog.aspx

From my point of view, have no significant difference between these 2 packages but my suggestion is the latest version.

Nhi_Nguyen_0-1695364478081.png

Best regards,

Nhi

0 件の賞賛
返信