S32K Crystal Drive, Gain Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K Crystal Drive, Gain Control

跳至解决方案
3,248 次查看
patricklanglois
Contributor II

Hi,

Looking at the datasheet, reference manual and application notes for the S32K microcontrollers, I can't understand if there is a minimum automatic gain control additionally to the programmable one (HI/LO gain) for an external crystal drive (SOSC).

To be as clear as possible...

For each range of crystal frequencies "covered" by each of both manual gain settings, is there some automatic control that will increase the crystal drive to provide a proper level of response on the inverter input?

Regards.

1 解答
3,129 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Patrick Langlois

Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.  When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.

Regards

Jorge Alcala

在原帖中查看解决方案

1 回复
3,130 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Patrick Langlois

Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.  When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.

Regards

Jorge Alcala