S32K CMP roundrobin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K CMP roundrobin

2,367件の閲覧回数
bastih84
Contributor I

Hi,

How can I use roundrobin mode for four channels (if possible without interrupts) with S32K.

I use NXP SDK's at the moment.

For one channel (without roundrobin and with interrupt) everything works fine.

Is there any example from somebody available? For roundrobin mode?

I will also use internal DAC, same limit for all channels.

Thanks a lot

Bastian

0 件の賞賛
返信
2 返答(返信)

2,141件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi Bastian,

At this moment we don't have any example with CMP in trigger mode/round robin.

I don't know your usecase, but is important to know that this CMP mode is available only if the MCU is STOP1 or VLPS and LPTRM must be used to trigger the CMP comparisons.

Best regards,

Razvan

0 件の賞賛
返信

2,141件の閲覧回数
youssef
Contributor II

Hi Rasvan,

Do you have any example about how to use CMP in trigger mode to wakeup S32 from VLPS?

I tried to configure LPTMR and CMP to work in round robin mode but no success yet.

Thanks,

Youssef

0 件の賞賛
返信