S32K 148 Bus error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K 148 Bus error

1,372件の閲覧回数
TerryDuPower
Contributor III

I debug flash driver, and get a exception. After that the Trace 32 shows bus error, and can't reprogramm.

How to recover it?

 

TerryDuPower_0-1691745262767.png

 

0 件の賞賛
返信
1 返信

1,340件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @TerryDuPower,

Does this happen during the Startup, during the run time of the application or during a flash operation?

I would recommend implementing the HardFault_Handler() in the project, and debug it as it is shown here:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

What kind of bus fault is it?

If a precise fault, what is the content of the BFAR register?

 

Thanks,

BR, Daniel

 

0 件の賞賛
返信