S32Design Studio make error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32Design Studio make error

Jump to solution
1,992 Views
OTSL-J
Contributor III

When installing the Windows version of S32Design Studio and building our project the following error occurred.

-----
make -j12 all
1 [main] make 1916 dofork: child -1 - forked process 7660 died unexpectedly, retry 0, exit code 0xC0000142, errno 11
make: *** [src/subdir.mk:57: src/DipSW.o] Error 127
Build might be incomplete.
-----

The version of S32Design Studio is 3.5.
The following additional packages were installed.
 S32 Design Studio 3.5 Update 11 D2403
 S32K1xx development package
 S32SDK S32K1XX RTM

Some Windows PCs build successfully and some Windows PCs fail, so we cannot determine if we are missing any packages required to install S32Design Studio.
Can you please advise as to why the builds are failing?
Best regards.

0 Kudos
Reply
1 Solution
1,931 Views
jiri_kral
NXP Employee
NXP Employee

Perfect, thank you for sharing the solution! 

View solution in original post

0 Kudos
Reply
3 Replies
1,964 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please try to update S32DS to latest version - v3.5.14 . It looks that the issue is not related to any package/dependency. 

0 Kudos
Reply
1,944 Views
OTSL-J
Contributor III

Thank you very much.
I am pleased to report that I have resolved the issue myself.
Reference URL

'Error: Could not fork child process' while opening Sage - ASKSAGE: Sage Q&A Forum
I was able to build by following this procedure to turn off mandatory ASLR.

1,932 Views
jiri_kral
NXP Employee
NXP Employee

Perfect, thank you for sharing the solution! 

0 Kudos
Reply