S32DS setup for S32K144 help for simplest program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS setup for S32K144 help for simplest program

Jump to solution
1,981 Views
brucebowling
Contributor III

Been ripping my hair out trying to figure this out, I am sure I am missing something. Trying to get a simple program to compile, following the cookbook examples. I have installed the S32DS.3.5_b220726_win32.x86_64.exe and the SW32K1_S32DS_3.5.4_D2307.zip for the toolchain. Created a new project and selected S32K144 device. I am trying to compile this simple 1 line:

#include "S32K144.h"

int main(void) {

WDOG->CNT=0xD928C520;

}

Compiler says  error: 'WDOG' undeclared - this syntax comes straight out of the cookbook.  Obviously I do not have the correct include file or there has been a change, what am I missing? Do I need to install the SDK and/or the RTM in order to get this one simple line to compile? I have read many help pages and posts but have not found anything specific to this issue. I know I am missing something, anyone know? Thanks - Bruce

0 Kudos
Reply
1 Solution
1,947 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @brucebowling 

The definition of the Peripheral WDOG base pointer (WDOG) has changed in the S32DS v3.5 ".h" files, now defined as "IP_WDOG". This also applies to all the definitions of the peripherals base pointer.

Please check these changes directly in the "S32K144.h".

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
1 Reply
1,948 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @brucebowling 

The definition of the Peripheral WDOG base pointer (WDOG) has changed in the S32DS v3.5 ".h" files, now defined as "IP_WDOG". This also applies to all the definitions of the peripherals base pointer.

Please check these changes directly in the "S32K144.h".

 

B.R.

VaneB

0 Kudos
Reply