[S32DS for S32K1] JSCOPE equivalent functionality for debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32DS for S32K1] JSCOPE equivalent functionality for debug

2,751件の閲覧回数
narsimh_kamath
NXP Employee
NXP Employee

Dear Team,

A customer working with S32K144 & trying to adopt S32DS has the following question, " Similar to J-scope, logical analyzer (communication protocols,- Minimum 100MHz Bandwidth), live variables viewer GUI (I have not found in IDE S32 Design Studio, but it is available in IAR IDE ), etc., any of these available from NXP, which should be very ease to handle and configure, can be interfaced to the existing screen (Laptop screen, Smartphone screen etc.)"

Essentially, the customer needs real-time view into a large number of internal variables (numbering ~50) and finds that Segger JSCOPE with IAR was very good. What toolchain (debugger/plug-in, etc.) can help this customer achieve equivalent functionality with S32DS for S32K1? 

Thanks & Regards,

Narsimh

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,712件の閲覧回数
narsimh_kamath
NXP Employee
NXP Employee

Thanks @Senlent ! 

  • Is there a specific debugger and any specific debug interface of S32K1 that is needed for the approach you outline above?
  • Does it have any constraint in terms of number of variables that can be viewed in real-time?
0 件の賞賛
返信

2,705件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@ narsimh_kamath

The debugger is the J-LINK series from SEGGER, such as J-LINK PRO or Plus, etc.

For more details you need to seek technical support from SEGGER.

https://www.segger.com/products/debug-probes/j-link/tools/j-scope/

Senlent_0-1708926853900.pngSenlent_0-1708926853900.png

You can see that the number of variables and sampling rates that different J-LINKs can support for observation are quite different.

0 件の賞賛
返信

2,717件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@narsimh_kamath

The S32 DS does not have such a GUI to view variable waveforms, but J-SCOPE is a third-party tool that can still be used with the S32 DS.

You only need to import the ELF file.

Senlent_0-1708914977039.pngSenlent_0-1708914977039.png

Senlent_1-1708915095260.pngSenlent_1-1708915095260.png

Senlent_2-1708915101524.pngSenlent_2-1708915101524.png

 

 

 

0 件の賞賛
返信