S32DS V3.4 about Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS V3.4 about Configuration

Jump to solution
1,769 Views
NewMCU
Contributor I

It was developed with S32K144. Help -> Installation Details -> New configuration update, but driver end cannot be added anymore.

For example, an existing code was initially set in pin 9.0, but if you update it to pin V10.0, and then add a driver end, the following error occurs.

Can't S32DS

NewMCU_0-1683187481925.png

NewMCU_1-1683187498575.png

 

 

V3.4 update the Configuration?

0 Kudos
Reply
1 Solution
1,754 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @NewMCU 

I'm afraid the description is not very clear to me. Do you port a project from another version of S32 Design Studio? Or from another version of SDK?

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
1,755 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @NewMCU 

I'm afraid the description is not very clear to me. Do you port a project from another version of S32 Design Studio? Or from another version of SDK?

Regards,

Lukas

0 Kudos
Reply