S32DS V3.4 about Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS V3.4 about Configuration

ソリューションへジャンプ
1,766件の閲覧回数
NewMCU
Contributor I

It was developed with S32K144. Help -> Installation Details -> New configuration update, but driver end cannot be added anymore.

For example, an existing code was initially set in pin 9.0, but if you update it to pin V10.0, and then add a driver end, the following error occurs.

Can't S32DS

NewMCU_0-1683187481925.png

NewMCU_1-1683187498575.png

 

 

V3.4 update the Configuration?

0 件の賞賛
返信
1 解決策
1,751件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @NewMCU 

I'm afraid the description is not very clear to me. Do you port a project from another version of S32 Design Studio? Or from another version of SDK?

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,752件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @NewMCU 

I'm afraid the description is not very clear to me. Do you port a project from another version of S32 Design Studio? Or from another version of SDK?

Regards,

Lukas

0 件の賞賛
返信