S32DS- Support for WolfSSL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS- Support for WolfSSL

2,693件の閲覧回数
biju_nair
Contributor III

Hi,

I am using S32DS-3.5 and developing application for S32K314 MCU. The SDK that is being used is PlatformSDK_S32K3_2022_07. I would like to use WolfSSL in my application. I saw some post on WolfSSL with S32DS, but it was not very clear. Can someone help me answer the following queries.

 

1. Is wolfSSL bundled by default in PlatformSDK_S32K3_2022_07 be default ?

2. If no, then how can i get WolfSSL libraries into my existing project ?

3. Is there any stand alone WolfSSL library project for S32DS available for download ? I checked wolfSSL site and they dont have any projects for S32DS. Its available for MCUXpresso and lot of other tools.

Any help is highly appreciated.

Regards, Biju

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,656件の閲覧回数
PZsolt
Contributor I

Hi Lukas!

I have a s32k3x8evb (k358) board and want to use wolfssl. I have downloaded the version 1.0.4 (because I have RTD 4.X and Freertos 10.6 already), but I can't find wolfss? Is it no more included in the stack?

 

Screenshot 2025-02-03 182240.png

0 件の賞賛
返信

2,655件の閲覧回数
biju_nair
Contributor III

Thank you very much. Appreciate your help.

Regards, Biju

0 件の賞賛
返信

2,672件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @biju_nair 

wolfssl is integrated to TCPIP stack which can be found in S32K3 Reference Software:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D

Currently there's version 1.0.1 which can be used with S32 Design Studio 3.4 and RTD 2.0.1. See please release notes for details about the installation and compatibility and then also TCPIP user manual after installation.

Regards,

Lukas

0 件の賞賛
返信