S32DS Platform for S32K144 initial setup problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Platform for S32K144 initial setup problems

1,245 Views
aneurauter
Contributor II

I am following this article HOWTO: Create a Blinking LED example project using... - NXP Community to start a project using SDKs RTMs RTDs. 
I followed the initial installation steps outlined in installation guide found on the same software download page as the S32DS installer and SW32K1_S32DS_3.5.4_D2307. I pointed the extensions updates page to the zip file for SW32K1_S32DS_3.5.4_D2307 and the zip file for SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite. The S32SDK_S32K1xx_RTM_4.0.2 is installed in the same top level NXP folder as the IDE.

 

When I follow the instructions to create a Blinky light with the AUTOSAR drivers, I get the following error after turning off the Pins too as instructed in the HOW TO page. 

aneurauter_0-1698161445075.png

I am unable to complete the HOW TO document as the project will not build and would like to know which step I have missed or what I haven't installed. 

 

0 Kudos
Reply
2 Replies

929 Views
aneurauter
Contributor II

Problem was unknowingly using a 144W chip. The 144 initial project configurations and 144W initial project configurations are different

0 Kudos
Reply

1,197 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @aneurauter 

I'm not able to replicate the issue, I followed the HOWTO you were using and I did not face any problem. Have you tried to create the project from an example instead?

Also I would like to see the installations details of your ide to verify that everything is correct, can you provide them please?

Let me know.

Best Regards, Miguel.

0 Kudos
Reply