S32DS Error when add Fee module for S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Error when add Fee module for S32K312

659件の閲覧回数
Jojo_Hu
Contributor II

你好,

在S32DS的工程环境中,当添加了模块Fee时,显示如下错误,进而无法生成代码。请问是环境的问题吗,是否仍有某个插件需要被安装?

期待您的解答。

Jojo_Hu_0-1748342045065.png

 

0 件の賞賛
返信
4 返答(返信)

635件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jojo_Hu 

I used Copilot to help translate the error message shown by S32DS, and it looks like the issue might be related to missing or misconfigured SDK components.

To help figure out what is going on, could you please share the following information?

  • Device are you working with.  I noticed that the image refers to Core 0, but you mentioned the device is single core device, so I am a bit confused. Could you clarify that part?
  • Which software and version are you using?
  • Could you share some details about your S32DS installation details?
  • Did you create the project from scratch, or did you import it into your workspace?

This will help us narrow down the possible causes. 

 

BR, VaneB

0 件の賞賛
返信

623件の閲覧回数
Jojo_Hu
Contributor II
  • Device are you working with.  I noticed that the image refers to Core 0, but you mentioned the device is single core device, so I am a bit confused. Could you clarify that part?

         ------- Device: The hardware board we designed ourselves has an MCU of S32K312.

  • Which software and version are you using?

         ------- S32DS.3.4_b201217_win32.x86_64.exe, this is what we installed.

  • Could you share some details about your S32DS installation details?

         ------- Jojo_Hu_0-1748397810900.png

 

  • Did you create the project from scratch, or did you import it into your workspace?

         ------- the project was created from scratch by my colleagues. We installed the software with same steps. The "FEE" module encountered this error prompt the first time it was added by me, but my colleague didn't meet this issue

0 件の賞賛
返信

616件の閲覧回数
Jojo_Hu
Contributor II

After reinstalling the software, everything seems normal

596件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @Jojo_Hu 

Glad to hear that. If any other issues come up or if this one happens again, feel free to let me know.

0 件の賞賛
返信