S32DS Compilation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Compilation problem

3,541 Views
xxw1
Contributor I
First of all I just used this software for a week
and i use S32K146 for my work , i transplant the Linux kernel file list.h.
Failure to compile occurred. Locate to “container_of ”
I'd like to ask how to compile. Is it caused by non ‘GNU C’ compilation? If so, how to configure it.
Thank you!
0 Kudos
Reply
3 Replies

3,514 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@xxw1

There are some help documents in the installation directory to help you how to use the S32 DS IDE.

help files path:for example.

.....\S32DS_ARM_v2.2\S32DS\help\pdf

Regarding your question, the transplantation of third-party files, we are unable to provide you with effective advice and assistance. If you have any usage problems, such as working abnormally or you don't understand how to use certain functions,please describe your problem clearly, we will help you answer in time.

BR!

     Jim,

0 Kudos
Reply

2,533 Views
fisherwky
Contributor I
 
0 Kudos
Reply

3,508 Views
xxw1
Contributor I

Thank you for your answer, but it didn't solve my problem

Pdf page 140 describes“

The language standard to which the code should conform. The compiler accepts

all programs that follow the specified standard plus GNU extensions that do not

contradict it.

”

What does this mean and does the software support the GNU extended language standard?

If the GNU extension language standard is supported, how can I configure it

I can only configure“C language: ISO C90/ANSI C89 (-std=c90), ISO C99 (-std=c99), ISO

C11 (-std=c11)”

I need GNU extended.

thank you

0 Kudos
Reply