S32 design example project UM11965 throws error while building project - CANHUBK344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design example project UM11965 throws error while building project - CANHUBK344

1,575 Views
Prasanna2
Contributor I

I am following Section 8 of UM 11965 (CANHUBK344), successfully did a offline install of the extensions & imported the sample project and did a build project. It throws multiple errors for the TODOs .. What should we do with the TODOs here, i have the reference kit hardware and in the user manual no mention of these TODOs.  And also once i build the project could you share the link of how to flash the elf file using programmer ?

Prasanna2_0-1757446089919.png

 

0 Kudos
Reply
5 Replies

1,501 Views
Prasanna2
Contributor I

Sorry let me rephrase my issue. The main issue relating to the build errors while compiling the sample code for CANHUBK344. I am following Section 8 of UM 11965 (CANHUBK344) &  imported the sample project and did a build project. It throws multiple compilation errors for the TODOs in the sample code MR_CANHUBK3_IEEE1722   .. What should we do with the TODOs in the sample code here, i have the reference kit hardware and in the user manual no mention of these TODOs.  How do i fix this compilation errors refer below the screentshot sample

Prasanna2_0-1757565705743.png

 

0 Kudos
Reply

1,494 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am able to build this project without error

Build Finished 0 errors MR_CANHUBK3_IEEE1722.png

0 Kudos
Reply

1,521 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

There is no on-board debugger on the CANHUBK344 board. Did you connect external debugger(PEMicro Multilink or Segger J-Link) at P7A?

MR-CANHUBK344 external 12V and Multilink FX debugger - Copy.jpg

If you are using Segger J-Link, please refer to S32 Design Studio for S32 Platform V3.4/V3.5 + SEGGER J-LINK Plus

If you are using PEMicro Multilink, please refer to

PEMicro debug.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,430 Views
Prasanna2
Contributor I

Hello ,

Could you advise which is best option for programming & debugging ?

- PEM Micro Multi Link 

- J-LINK

Or MCU-Link Debug probe

Or other option 

Apart from flashing/programming i also want the better capabilities for debugging ..

0 Kudos
Reply

1,374 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Lauterbach TRACE32
PEMicro Multilink
SEGGER J-Link

0 Kudos
Reply