S32 Series MCU : Difference between ADC Precise Input and ADC Standard Input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Series MCU : Difference between ADC Precise Input and ADC Standard Input

3,463 次查看
Sreelakshmi
Contributor I

Dear Team,

While referring the S32 series MCU IO Mux sheet, I could see that some ADC Inputs are described as ADC Precise Input and some as ADC Standard Input.

What is the difference between the two?

Regards

Sreelakshmi A

0 项奖励
回复
3 回复数

3,244 次查看
Sreelakshmi
Contributor I

Hi Vane,

Thanks for the details.

I would also like to know the difference between External ADC Input Pin.

How is it different from Precise and Standard ADC Input Pins.

Regards

Sreelakshmi A

0 项奖励
回复

3,214 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Sreelakshmi 

Please check the following link. There is information related to the topic you might find useful. 

S32K3 ADC Use of external channels

0 项奖励
回复

3,445 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Sreelakshmi 

The precision channels have fewer parasitics than standard channels. The external channels are channels using an external analog mux supported by the ADC. Most parasitics are dominated by the external circuit (varied by the design).

Also, the precision channels have a capacitance of 0.57pF (ADC0), 1.34pF (ADC1), and 1.32pF (ADC2). The standard channels have 4.18/4.13/4.03pF respectively.

Another important consideration is the TUE, reported in the DS is equal for all channel types (Precision Standard and External).

The DS specification: Typ TUE(+/-4 LSB) and Max TUE(+/-6 or +/-8 LSB depending on condition) applies to all channel types (Precision Standard and External), but is important to take into consideration that the specifications apply only to the MCU (The accuracy dropping for an external MUX component needs to be considered a part of the S32K3xx DS). 

 

B.R.

VaneB

0 项奖励
回复