S32 K312 Stuck in RAM initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 K312 Stuck in RAM initialization

256 次查看
Jianfeng2
Contributor I

Dear supporter,

        We use S32 312k, compiler is IAR. The bootloader the Occasionally stuck and not response any Diagnostic request. After Power on reset, the issue recovered.

       1. When issue reproduced, attached Trace 32, the program stopped in brsStartupEntry().

Jianfeng2_0-1742951978267.png

2. Check the Trace list, the last command is initializing the RAM

Jianfeng2_1-1742952114260.png

Jianfeng2_2-1742952537144.png

3. Check the map file. The RAM code is not 4byte alignment in map file.

Jianfeng2_3-1742952956644.png

 

My question:

Which kind fault can trigger initialize the RAM jump to  brsStartupEntry()?

If the RAM Code not 4- or 8-bytes alignment, what is the risk?

Is there any relationship between RAM Code not alignment and the stuck issue?

 

Thanks!

Best Regards!

 

 

 

 

0 项奖励
回复
0 回复数