S32_K144_bootloader Linker file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32_K144_bootloader Linker file

1,328件の閲覧回数
arun_07
Contributor I

Hi Team,

I ported my application from S32k144 to S32K142_64, but the S32K144_100 Project contains S32K144_64_flash_bootloader.ld, and I'm unable to generate this file for S32K142_64.

 

And One more issue I'm facing is that when I'm generating processor expert file I'm getting trgmux.chg undefined CPU type S32K142_64.

All suggestions are welcome.

Ta

0 件の賞賛
返信
1 返信

1,291件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

S32K144_64_flash_bootloader.ld is obviously customized linker file which is not generated by S32DS. If you are moving to another derivative, it will be necessary to manually update the linker file as needed (S32K142 has less RAM and flash).

Regards,

Lukas

0 件の賞賛
返信