S32 Development Studio 3.6.10 RTD Installation failed Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Development Studio 3.6.10 RTD Installation failed Error

236 Views
shyam_tayade
Contributor I

Hello,

I have successfully installed S32 Design Studio (S32DS) v3.6.10 and am currently trying to install RTD v5.0.0 using the package:

S32K3XX_S32M27x_RTD_R21-11_5.0.0_P08_D2504_DesignStudio_updatesite.zipRTD_error.pngRTD_error.png

However, during the installation process, I am encountering errors, which are captured in the attached document.

I am using an S32K3 Automotive Telematics Box (T-Box) evaluation board and would like to set up a complete development environment on my system, including RTD, FreeRTOS/RTOS support, and the required toolchain and middleware components.

Could you please help me:

  1. Understand and resolve the installation errors shown in the attachment.
  2. Verify whether RTD 5.0.0 is compatible with S32DS v3.6.10.
  3. Recommend the correct RTD and FreeRTOS package versions for my board and development setup.
  4. Provide the recommended steps to complete the development environment setup, including any additional software, SDKs, or middleware that may be required.

Your guidance would be greatly appreciated.

Thank you, Shyam

0 Kudos
Reply
1 Reply

208 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Shyam,

According to page 12 of S32K3 Automotive Telematics Box (T-Box) lwIP Example Guide Training Presentation[TP-S32K3-T-BOX-LWIP-GUIDE] those software need to be installed:

 

However, as far as I know, these software versions were released a long time ago, and you may not have permission to download such old versions.

Please wait while I apply to the internal team for download permissions for these older software versions for your account.

Since I'm unsure if your account can currently download these software, please try the following link to see if you can download them: 

click S32 Design Studio – Windows/Linux -> S32 Design Studio IDE -> Previous -> S32 Design Studio for S32 Platform v.3.4 -> S32DS.3.4_b201217_win32.x86_64.exe
click S32 Design Studio – Windows/Linux -> Automotive SW - S32K3 - S32 Design Studio > Previous -> 3.4.3_D2112 S32 Design Studio for S32 Platform v.3.4 Update 3 with support for S32K3 devices -> SW32K3_S32DS_3.4.3_D2112.zip

 

For S32K3 Automotive Telematics Box (T-Box) lwIP Example Code for S32K3 Code Snippets S32K3-T-BOX-LWIP-FOR-S32K3 Please download below software package:
click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> 2.0.0 S32K3 Real Time Drivers Version 2.0.0 -> SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip

click S32K3 Standard Software -> Automotive SW - S32K3 - FreeRTOS -> Previous -> 2.0.0 SW32K3_FreeRTOS_10.4.6_2.0.0_D2204 -> SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip

click S32K3 Standard Software -> Automotive SW - S32K3 - Stacks -> 1.0.1 SW32K3_TCPIP_STACK_1_0_1_D2205 -> S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip

 

For S32K3 Automotive Telematics Box (T-Box) BSPs, Drivers and Middleware S32K3-T-BOX-BSP
Please download below software package:
click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M -> 1.0.0_HF02 S32K3 Real Time Drivers Version 1.0.0 HotFix 02 -> SW32K3_RTD_4.4_1.0.0_HF02_DS_updatesite_D2112.zip

click S32K3 Standard Software -> Automotive SW - S32K3 - FreeRTOS -> Previous -> 1.0.0 SW32K3_FreeRTOS_10.4.5_1.0.0_D2110 -> SW32K3_FreeRTOS_10_4_5_UOS_1_0_0_DS_updatesite_D2110.zip

click S32K3 Standard Software -> Automotive SW - S32K3 - Stacks -> 1.0.0 SW32K3_TCPIP_STACK_1_0_0_D2111 -> S32K3_TCPIP_RTM_1_0_0_D2111_updatesite.zip

Best Regards,
Robin

0 Kudos
Reply