S32 Design Studio v3.4 extension installation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio v3.4 extension installation problem

2,276 Views
michaelcr97
Contributor II

Hello everyone,

 

I get an error message when I try to install the extension S32k1xx development package:

Operation detailsSoftware being installed: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 Missing requirement: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.s32k1.s32k142w.dev.feature.feature.group [1.0.0.202106101446,1.0.0.202106101446]' but it could not be found

Can you help me please? Thank you!

0 Kudos
Reply
5 Replies

2,260 Views
Robert344Humphries
Contributor II

Hello!

It sounds like you're encountering an issue installing the S32k1xx development package due to a missing requirement. To resolve this, ensure that your SDK and related components are updated, verify all dependencies are installed, consider offline installation, review the documentation for additional steps, and reach out to Qualcomm support if the issue persists. 

2,216 Views
Robert344Humphries
Contributor II

Did you find it useful?

Best Regards,

Robert

MyFedLoan

0 Kudos
Reply

2,212 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Several customers have successfully installed it after making this modification. So please try it and let me know the results.

0 Kudos
Reply

2,232 Views
michaelcr97
Contributor II

Hello! As you said, I found that requirements aren`t installed. I tried to find those by google, but I didn`t. Can you help me with this please?

michaelcr97_0-1732442417253.png

 

0 Kudos
Reply

2,222 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It is recommended to change Available S32DS Software Sites to https. Please refer to the discussion in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply