S32 Design Studio - ld returned 5 exit status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio - ld returned 5 exit status

2,618件の閲覧回数
Durgaprasad02
Contributor II

 

Hi,

I'm encountering the following error during the build process:.

Invoking: Standard S32DS C Linker
arm-none-eabi-gcc -o "can_pal_s32k118.elf" "@can_pal_s32k118.args"
collect2.exe: error: ld returned 5 exit status
make: *** [makefile:47: can_pal_s32k118.elf] Error 1
make -j14 all" terminated with exit code 2. Build might be incomplete.

Could you please help me resolve this issue?

0 件の賞賛
返信
9 返答(返信)

2,562件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you share which version of S32DS you are using?

Best regards,

Peter

 

0 件の賞賛
返信

2,553件の閲覧回数
Durgaprasad02
Contributor II

Durgaprasad02_0-1742531232268.png

 

0 件の賞賛
返信

2,546件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share full output from build console? 

 

If you delete (or make backup and delete it from workspace, if it is modified example) the project and create it again from File -> Project from Example, is the behavior same? If So, try to create new workspace. 

0 件の賞賛
返信

2,537件の閲覧回数
Durgaprasad02
Contributor II

Hi jiri,

Please find attached console data  for your reference.

タグ(1)
0 件の賞賛
返信

2,521件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Everything looks okay, except the linker error. 

Please try another example or create new workspace and open again can_pal example in new workspace. 

0 件の賞賛
返信

2,509件の閲覧回数
Durgaprasad02
Contributor II
Hi Jiri,

getting same.
0 件の賞賛
返信

2,379件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

were you able to resolve the issue or it is the same.

Did you try it also on different PC?

best regards,

Peter

0 件の賞賛
返信

2,586件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hard to say, you can try to enabled verbose mode and put whole output from build console.

petervlna_0-1742458179375.png

Best regards,

Peter

 

0 件の賞賛
返信

2,578件の閲覧回数
Durgaprasad02
Contributor II

Hello peter,

Same error after enabling that check box too.

0 件の賞賛
返信