S32 Design Studio for S32 Platform 3.4 running error!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for S32 Platform 3.4 running error!

ソリューションへジャンプ
3,858件の閲覧回数
mark14
Contributor II

The error dialog box:

mark14_0-1694063904427.png

The error log:

!SESSION 2023-09-07 11:43:47.807 -----------------------------------------------
eclipse.buildId=3.4.0.202012171340
java.version=1.8.0_202
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=zh_CN
Command-line arguments:  -os win32 -ws win32 -arch x86_64
 
!ENTRY org.eclipse.tools.templates.freemarker.java11 2 0 2023-09-07 11:43:52.696
!MESSAGE Could not resolve module: org.eclipse.tools.templates.freemarker.java11 [709]
  Unresolved requirement: Fragment-Host: org.eclipse.tools.templates.freemarker; bundle-version="1.0.0"
 
 
!ENTRY org.eclipse.osgi 4 0 2023-09-07 11:43:52.698
!MESSAGE Application error
!STACK 1
org.apache.batik.css.parser.ParseException: identifier.character
at org.apache.batik.css.parser.Scanner.nextToken(Scanner.java:774)
at org.apache.batik.css.parser.Scanner.next(Scanner.java:222)
at org.apache.batik.css.parser.Parser.parseStyleSheet(Parser.java:185)
at org.eclipse.e4.ui.css.core.impl.dom.parsers.AbstractCSSParser.parseStyleSheet(AbstractCSSParser.java:63)
at org.eclipse.e4.ui.css.core.impl.engine.AbstractCSSEngine.parseStyleSheet(AbstractCSSEngine.java:187)
at org.eclipse.e4.ui.css.swt.internal.theme.ThemeEngine.setTheme(ThemeEngine.java:474)
at org.eclipse.e4.ui.css.swt.internal.theme.ThemeEngine.setTheme(ThemeEngine.java:435)
at org.eclipse.e4.ui.css.swt.internal.theme.ThemeEngine.setTheme(ThemeEngine.java:412)
at org.eclipse.e4.ui.css.swt.internal.theme.ThemeEngine.restore(ThemeEngine.java:613)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.setCSSTheme(PartRenderingEngine.java:1427)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.initializeStyling(PartRenderingEngine.java:1334)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1053)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1049)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:660)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:559)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:154)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:150)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:137)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:107)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:657)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:594)
at org.eclipse.equinox.launcher.Main.run(Main.java:1465)
 
Thanks
0 件の賞賛
返信
1 解決策
3,455件の閲覧回数
mark14
Contributor II

The error has been resolved, it is due to the company's security policy.

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,456件の閲覧回数
mark14
Contributor II

The error has been resolved, it is due to the company's security policy.

Thanks

0 件の賞賛
返信
3,457件の閲覧回数
mark14
Contributor II

The problem has been resolved, it is due to the company's security policy.

Thanks

3,777件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @mark14 , 

 

It looks like error because of multiple version of Java installed or not incompatible version of java installed on your computer. 

 

Please can you reinstall the design studio and try if works or not. That may fix the issue. 

 

Thank you. Kind regards. 

 

- Mehul Patel

0 件の賞賛
返信
3,547件の閲覧回数
mark14
Contributor II

I reinstalled both JAVA and S32 IDE, but the same error still occurred.

Thanks

0 件の賞賛
返信
3,485件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

please try to remove your existing Java installations and re-install S32DS. There is probably some mess in Environment Java path variables. 

0 件の賞賛
返信
3,722件の閲覧回数
mark14
Contributor II

Hi @Mehul_Patel_NXP 

This is the JAVA environment installed on my computer. Do I need to uninstall one or install JDK 8?

 

mark14_0-1694265074964.png

Thanks

0 件の賞賛
返信