S32 Design Rolling Back Installation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Rolling Back Installation error

1,916件の閲覧回数
Saisreeram
Contributor I

While trying to install S32 Design, at 6% installation it is showing an error as Installation Rolling back.

0 件の賞賛
返信
3 返答(返信)

1,839件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

based on info from log file, S32DS installer don't have enough privileges to write executable files and the installation is rolled back. Please make sure, that you are starting installation with admin rights and you are allowed to write executable files into C:\Users\mobis\AppData\Local\Temp\ folder. 

0 件の賞賛
返信

1,906件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

From your description is impossible to tell you what is the issue.

Could you share at least some screenshots of the issue?

Best regards,

Peter

0 件の賞賛
返信

1,894件の閲覧回数
Saisreeram
Contributor I

Hello
While Installing S32 Design V3.4, at 6% installation point, it says that the installation rolling back.
I have attached the log file for the info, Could you please check and help me..

0 件の賞賛
返信