S32 Design Rolling Back Installation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Rolling Back Installation error

1,975 Views
Saisreeram
Contributor I

While trying to install S32 Design, at 6% installation it is showing an error as Installation Rolling back.

0 Kudos
Reply
3 Replies

1,898 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

based on info from log file, S32DS installer don't have enough privileges to write executable files and the installation is rolled back. Please make sure, that you are starting installation with admin rights and you are allowed to write executable files into C:\Users\mobis\AppData\Local\Temp\ folder. 

0 Kudos
Reply

1,965 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

From your description is impossible to tell you what is the issue.

Could you share at least some screenshots of the issue?

Best regards,

Peter

0 Kudos
Reply

1,953 Views
Saisreeram
Contributor I

Hello
While Installing S32 Design V3.4, at 6% installation point, it says that the installation rolling back.
I have attached the log file for the info, Could you please check and help me..

0 Kudos
Reply