Hi,
New to the S32K DS v3.5 and am trying to get some code working with FreeRTOS for the S32K344.
Where can i find some example projects?
Or Do i need to install additional package? if so can anyone share me the links?
Thanks in advance
Solved! Go to Solution.
OK, then download "FreeRTOS 10.6.0 version 4.0.0"
BR, Petr
View solution in original post
yes, to get FreeRTOS example you need to add FreeRTOS package on top of RTD one. After successful installation you would be able to create new project from demo examples
You did not specify the RTD version you have installed, based on this you need to select right FreeRTOS package version from https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D
Read package release note document for more info about installation steps and required prerequisites.
Hi @PetrS ,
I am using RTD V 4.0.0.