Requesting for correct timing configuration parameter for I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Requesting for correct timing configuration parameter for I2C

4,329 Views
marotib
Contributor I

 Using S32K344 EV board for sensor interfacing via I2C channel. Operating frequency is 10 MHZ and I want to operate slave device in standard mode(100KHZ).

currently when I am transmitting data on SDA line but I don't see correct data.

So I think this is the issue with timing configuration, Can you please provide correct I2C timing configuration for above mentioned parameter ?

0 Kudos
Reply
2 Replies

4,284 Views
marotib
Contributor I

Thank you... let me check

0 Kudos
Reply

4,293 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please note the Table 421. LPI2C Timing Parameter Restrictions of S32K3XXRM.

Table 421. LPI2C Timing Parameter Restrictions.png

DATAVD Maximum CLKLO - SDA_LATENCY - 1. It does not meet.
BUSIDLE Minimum (CLKLO+SETHOLD+2) x 2. It does not meet.

I2C_TimingConfiguration - Copy.PNG


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply