Request for interrupt based FlexCAN reception example code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request for interrupt based FlexCAN reception example code

2,120 次查看
sachin922185
Contributor II

Hello Team,

We are using s32k344evb-q172 evaluation board. We want to perform the interrupt  based CAN reception but unfortunately there is no example code available for same.

Request you to please share the interrupt based FlexCAN reception example code.

Thanks & Regards,

Sachin N

@ndd922478 

0 项奖励
回复
3 回复数

2,085 次查看
sachin922185
Contributor II

Hello Petr,

Thanks for the reply.

I tried this example, but event is triggering once reception is completed from Mailbox to CPU.

Our use case is that there should be interrupt when message is just come into Mailbox.

Please guide on this, how we can achieve our use case?

 

Thanks & Regards,

Sachin N

0 项奖励
回复

2,073 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if using RTD driver, this is done that way, using callbacks. If you have e.g baremetal code then generally, the MB flag in IFLAG register is set when message is received/transmitted without error. If also MB mask bit is set in the IMASK register and interrupts are enabled in the core, the MB interrupt is called.

BR, Petr

0 项奖励
回复

2,108 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi, 

I placed some RTD based example on https://community.nxp.com/t5/S32K/FlexCAN-IP-example-not-running-in-normal-mode-on-S32K344-EVB/td-p/...
If you are using s32k344evb-q172 with TJA1043 you can skip transceiver init within code.
In the code a callback is used to indicate MB interrupt.
Hope it helps 

BR, Petr

0 项奖励
回复