Request for interrupt based FlexCAN reception example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request for interrupt based FlexCAN reception example code

2,172件の閲覧回数
sachin922185
Contributor II

Hello Team,

We are using s32k344evb-q172 evaluation board. We want to perform the interrupt  based CAN reception but unfortunately there is no example code available for same.

Request you to please share the interrupt based FlexCAN reception example code.

Thanks & Regards,

Sachin N

@ndd922478 

0 件の賞賛
返信
3 返答(返信)

2,137件の閲覧回数
sachin922185
Contributor II

Hello Petr,

Thanks for the reply.

I tried this example, but event is triggering once reception is completed from Mailbox to CPU.

Our use case is that there should be interrupt when message is just come into Mailbox.

Please guide on this, how we can achieve our use case?

 

Thanks & Regards,

Sachin N

0 件の賞賛
返信

2,125件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if using RTD driver, this is done that way, using callbacks. If you have e.g baremetal code then generally, the MB flag in IFLAG register is set when message is received/transmitted without error. If also MB mask bit is set in the IMASK register and interrupts are enabled in the core, the MB interrupt is called.

BR, Petr

0 件の賞賛
返信

2,160件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi, 

I placed some RTD based example on https://community.nxp.com/t5/S32K/FlexCAN-IP-example-not-running-in-normal-mode-on-S32K344-EVB/td-p/...
If you are using s32k344evb-q172 with TJA1043 you can skip transceiver init within code.
In the code a callback is used to indicate MB interrupt.
Hope it helps 

BR, Petr

0 件の賞賛
返信