Request access to the SafeAssure NDA group

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request access to the SafeAssure NDA group

2,016 次查看
EverettRao
NXP Employee
NXP Employee

I am everett a fae of nxp,I need request access to the SafeAssure NDA group to support our customers

标记 (1)
0 项奖励
回复
4 回复数

1,693 次查看
RandyZM
Contributor I

I'm FUSA engineer of Valeo  Interior Controls (Shenzhen) Co.,Ltd.

There's ASILD project using two ASILB MCU, one of two is MC2: FS32K116BRT0VLFR which is used for slave function. 

for MC2, no CAN transmission, just have the communication with MC1, MC1 send out the CAN message.

so there're some SMs and functions not implemented, need NXP help to re-calculate the MC2 FMEDA.

1. SM_075&SM_076 are not implemented. no CAN message leads to remove external clocks replaced by MC2 internal clock. MC2 internal clock accuracy ensured by MC1 synchronize;

2. SM_114 is not implemented, because no FUSA data is stored in EEPROM;

3, no eDMA transmission, just use CPU transmission.

Please help to re-calculate the MC2 FMEDA.

thanks~

 

0 项奖励
回复

1,678 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@RandyZM

Sorry for not being able to answer your question.


You can ask questions about functional safety in this forum

https://community.nxp.com/t5/SafeAssure-Community-Knowledge/REQUESTING-ACCESS-for-Safety-material-at... 

or get support from these channel.

submit a  ticket from the link below.

https://www.nxp.com/support/support:SUPPORTHOME

 

0 项奖励
回复

2,012 次查看
Senlent
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,988 次查看
EverettRao
NXP Employee
NXP Employee

thanks,solved 

0 项奖励
回复