Request S32K3 MCAL FlexCAN Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request S32K3 MCAL FlexCAN Example

4,603件の閲覧回数
dnewbe
Contributor III

Do you have a FlexCAN example made by MCAL driver on S32K344-EVB ?

 

I'm developing a FlexCAN example on S32K3X4EVB-Q257 board. The example code is made by MCAL driver. But that example (CAN_example_CT.mex) is work on Loopback mode and Polling operation. I did modify that example to not Loopback using CAN0 pins. 

So I verified basic operation using CAN API (Can_MainFunction_Write, Can_MainFunction_Read).

But the configuration of FlexCAN is works on one kind of Message ID. When config is Standard Message ID the Extended ID can't works. When config is Extended ID the Standard ID can't works.

I confuse relation between Message ID and Message Buffer (MailBox). For more Message ID and StandardFifo, LegacyFifo and ExtendedFio.

Could you tell me how to works Standard ID and Extended ID ?

 

My development is base on following.

- S32DS 3.4

- SDK is PlatformSDK_S32K3_2022_07

 

Thanks.

0 件の賞賛
返信
3 返答(返信)

4,562件の閲覧回数
dnewbe
Contributor III

Thanks PetrS

 

But I need MCAL driver because I did make other driver is make with MCAL driver like as LIN and PIT etc.

 

Thanks

0 件の賞賛
返信

4,557件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

4,589件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

could below example be helpful?
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test...
But it is using FlexCAN IP driver.

BR, Petr

0 件の賞賛
返信