Regarding trouble getting a software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding trouble getting a software

2,164 Views
patea202
Contributor I

I want "Automotive SW – EB tresos Studio / AUTOSAR Configuration Tool" under  "Automotive SW – S32K3 Standard Software". Please help me get this software. (This would be found under product list).

0 Kudos
Reply
4 Replies

2,111 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry I didn't understand your question. EB Tresos software can be downloaded here: S32K3 Standard Software -> Automotive SW - EB tresos Studio / AUTOSAR Configuration Tool -> EB tresos Studio 29.0.0

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,675 Views
aueranna
Contributor I

The user is requesting assistance in obtaining the “Automotive SW – EB tresos Studio / AUTOSAR Configuration Tool” software, which they believe is located under the “Automotive SW – S32K3 Standard Software” product list.

 

Geometry Dash

0 Kudos
Reply

1,665 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry, I didn't understand your question. Customers just need to click on S32K3 Standard Software to enter. I also suggest you raise a new question in the community.

0 Kudos
Reply

2,145 Views
aisha85adams
Contributor I

It's important to understand the relationship between "Automotive SW – S32K3 Standard Software" and "Automotive SW – EB tresos Studio / AUTOSAR Configuration Tool." Here's a breakdown:

S32K3 Standard Software:
This refers to the software provided by NXP Semiconductors for their S32K3 microcontroller series. It includes drivers, libraries, and tools to help developers build automotive applications.
EB tresos Studio / AUTOSAR Configuration Tool:
This is a software tool from Elektrobit (EB) used for configuring and generating AUTOSAR basic software (BSW). AUTOSAR (AUTomotive Open System ARchitecture) is a standardized software architecture for automotive ECUs (Electronic Control Units).
EB tresos Studio is often used in conjunction with microcontroller-specific software, such as the S32K3 standard software. It helps to configure the BSW components that interact with the microcontroller's hardware.
Essentially tools like EB tresos, are used to configure the AUTOSAR BSW, and that BSW will then be utilized on hardware, such as the NXP S32K3 microcontrollers. So they are tools that are used in the development process of the S32K3 software.
Here's how these elements relate:

When developing AUTOSAR-compliant software for an S32K3 microcontroller, developers often use EB tresos Studio to configure the AUTOSAR BSW.
The generated BSW code then interacts with the S32K3 standard software (drivers, etc.) to control the microcontroller's hardware.
To obtain EB tresos Studio, you would typically:

Contact Elektrobit directly through their website (elektrobit.com).
In some cases, semiconductor vendors like NXP may provide information or links to compatible AUTOSAR tools.
It is also worth noting that information from ST microelectronics, shows that they also support EB tresos studio with their microcontrollers.
Key points:

EB tresos Studio is a tool for AUTOSAR configuration.
S32K3 standard software is the software package for NXP's S32K3 microcontrollers.
These items are used in conjunction with each other, in the automotive software development process.
I hope this helps.

www pikepass com

0 Kudos
Reply