Regarding the demo program for S32K116, it is not functioning properly.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Regarding the demo program for S32K116, it is not functioning properly.

跳至解决方案
1,949 次查看
Haffman
Contributor I

HI

I'm using the lin_slave_baremetal_s32k116 sample program for debugging on the S32K116-Q048 demo board. However, the LIN interrupt is not working as expected. Here are the details: I have the S32K116-Q048 as the slave node, and a PC as the master for LIN communication. After testing, the LIN signal sent from the PC has been detected on GPIO PTC6, but the LIN interrupt is still not triggering. The power supply is at 12V. How can I resolve this issue?

BR

0 项奖励
回复
1 解答
1,875 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I tried lin_slave_baremetal_s32k116 demo example from SDK RTM4.0.3 on the S32K116EVB and it is working fine with mentioned PLIN View config. Callback (interrupt) is normally called and slave responds accordingly.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,902 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

have you sent right frames from PC's LIN tool as mentioned in example doxygen file? To have similar functionality as master example. See more in https://community.nxp.com/t5/S32K/S32K142-LIN-Setup/td-p/1477998

BR, Petr

0 项奖励
回复
1,899 次查看
Haffman
Contributor I

Dear Mr. Petr,

However, after my testing, the correct LIN signal has appeared on the corresponding GPIO, and the interrupt is triggered by the break signal. The program still cannot trigger the LIN interrupt. Then, when I send LIN data to S12 in the same way from my PC, S12 triggers the LIN interrupt normally.

BR

0 项奖励
回复
1,876 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I tried lin_slave_baremetal_s32k116 demo example from SDK RTM4.0.3 on the S32K116EVB and it is working fine with mentioned PLIN View config. Callback (interrupt) is normally called and slave responds accordingly.

BR, Petr

0 项奖励
回复