Regarding the Autosar Os_memmap error issue of S32k1xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding the Autosar Os_memmap error issue of S32k1xx

304 次查看
Lw2
Contributor III

 Hello! Thank you for taking the time to read this article.

            Let me describe the situation I encountered.I was creating an Autosar project using S32DS3.4. During the process, I encountered errors such as "Cannot find file Os_memmap.h" and other warnings, as shown in the following figure. Then I found the corresponding article on the forum. The cause of this problem is due to a mismatch between the Tresos RTD version and the RTD version installed on the S32DS.The library I use for EB is S32K1XX_MCAL4_2_RTM_1_0_6. For the S32DS 3.4 version, which RTD version should I install?Then where do I need to go to download it?

Lw2_0-1749465976253.png

The following are the libraries that I have already installed.

Lw2_1-1749466877611.png

Lw2_2-1749466923583.png

Lw2_3-1749466977916.png

 

 

 

 

0 项奖励
回复
2 回复数

279 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

S32K1XX_MCAL4_2_RTM_1_0_6. For the S32DS 3.4 version, which RTD version should I install?Then where do I need to go to download it?

S32K1XX_MCAL4_2_RTM_1_0_6. is some old release as I remember.

S32K1_S32M24x Real-Time Drivers AUTOSAR 4.4 - is latest one for S32K1 and it should be directly in the S32DS 3.6.2 supported.

I recommend you to install new S32design studio version 3.6.2.

Also there you can find the new RTD for S32k1.

petervlna_0-1749537619243.png

Best regards,

Peter

0 项奖励
回复

261 次查看
Lw2
Contributor III
Thank you very much for your reply. It will be of great help to me. I will try as you suggested first. Thank you.
0 项奖励
回复