Reflash Process

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reflash Process

1,964 次查看
emmanuelaguilas
Contributor II

Hello,

Before writing flash memory, is it recommended to verify the MCU source voltage to be into a minimal level?

Regards.

0 项奖励
回复
1 回复

1,903 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Emmanuel Aguilasocho

Device functionality is guaranteed up to the LVR assert level (2.7 V as Min.). So Inside the operating rating of the MCU, the device should operate correctly and the flash memory can be guaranteed.

Hope this helps.

Regards

Jorge Alcala

0 项奖励
回复