Reflash Process

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reflash Process

1,991件の閲覧回数
emmanuelaguilas
Contributor II

Hello,

Before writing flash memory, is it recommended to verify the MCU source voltage to be into a minimal level?

Regards.

0 件の賞賛
返信
1 返信

1,930件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Emmanuel Aguilasocho

Device functionality is guaranteed up to the LVR assert level (2.7 V as Min.). So Inside the operating rating of the MCU, the device should operate correctly and the flash memory can be guaranteed.

Hope this helps.

Regards

Jorge Alcala

0 件の賞賛
返信