Recovering from Secure Boot on S32K3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recovering from Secure Boot on S32K3

1,273件の閲覧回数
end48
Contributor I

Hello,

I'm currently implementing secure boot on a S32K310. I've got two questions:

  1. In case I configure secure boot on an SMR, how can I recover if the code in this SMR becomes corrupted? Do I need to flash with a debug probe the non corrupted firmware again? Is there another way?
  2. In case I need to modify the code in the SMR after activating the secure boot (during development typically), can I disable secure boot before updating the code and reconfigure secure boot on the new code?

Thanks,

Benoit

0 件の賞賛
返信
1 返信

1,212件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) You will have to update SMR if possible.

2) Once the secure boot is enabled, it can't be disabled.

0 件の賞賛
返信