Recover from Fatal error reading CPU status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recover from Fatal error reading CPU status

3,084件の閲覧回数
Hozumi
Contributor I

I'm trying to debug a S32K144 with IAR I-Jet, and first error1.png appears, then error2.png.
Is there any way to recover from this state?

error1 is "Do you want to perform mass erase to unlock the device"

After press "Yes", error2 will appear.
error2 is "Fatal error: Reading CPU status failed"

0 件の賞賛
返信
1 返信

3,062件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Hozumi,

Unfortunately, I am not familiarized with the IAR environment, but the probable cause for this error is that the security register was flashed with all values in F, which means the Flash Security register was set to 11b: MCU Security status is secure.

Julin_AragnM_0-1708364736580.png

Please try to mass erase unlock the device, and uncheck any secure chip option as shown in this other community: Solved: IAR appears do you want to perform mass erase to unlock the device?_iar do you want to perfo...

Julin_AragnM_4-1708364864056.png

Best regards,
Julián

0 件の賞賛
返信