Hi,team
I think there is no problem with my jump address, and the program may run away after the jump. My app program is with RTOS, while the boot program is without RTOS.The RTOS is dual stack, do the MSP and PSP need to be modified before the boot jumps to the application?
The ld file of boot:
/* Specify the memory areas */
MEMORY
{
 /* Flash */
 m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
 m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
 m_boot_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0000EF00
 m_app_text (RX) : ORIGIN = 0x0000F410, LENGTH = 0x000D0BF0
 /* SRAM_L */
 m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00008000
/* SRAM_U */
 m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x0000F000
}
the ld file of app:
/* Specify the memory areas */
MEMORY
{
 /* Flash */
 m_boot_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0000EF00
 m_interrupts (RX) : ORIGIN = 0x0000F000, LENGTH = 0x00000400
 m_flash_config (RX) : ORIGIN = 0x0000F400, LENGTH = 0x00000010
 m_app_text (RX) : ORIGIN = 0x0000F410, LENGTH = 0x000D0BF0
/* SRAM_L */
 m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
/* SRAM_U */
 m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x0000F000
}
Hello,
As you mention the PSP and the MSP should be modified before jumping to the application, the following routine corresponds to a bootloader example found in the Kinetis devices but the idea is the same for the S32K devices:
    shutdown_cleanup(kShutdownType_Shutdown); //disable the modules used in the bootloader
    static uint32_t s_stackPointer = 0;
    s_stackPointer = stackPointer;
    static void (*farewellBootloader)(void) = 0;
    farewellBootloader = (void (*)(void))applicationAddress;
    // Set the VTOR to the application vector table address.
    SCB->VTOR = (uint32_t)APP_VECTOR_TABLE;
    // Set stack pointers to the application stack pointer.
    __set_MSP(s_stackPointer);
    __set_PSP(s_stackPointer);
    // Jump to the application.
    farewellBootloader();I hope this helps you.
Best Regards,
Alexis Andalon
Hi,Alexis.
Thank you for your reply!Now my boot can jump to the app.However, when I jumped to boot from the app, the boot did not run successfully. Before judging this sentence, I used j-link to read the contents of memory. Both my boot and app were in the flash space I specified.When the app jumps to boot, I disallow watchdog and disallow global interrupt.The original software reset is able to achieve a direct jump to the boot, but the fact is not like this.I would like to ask whether it is related to RTOS, and whether there are any requirements on the stack between boot and app interchange. What work do I need to do before I can successfully realize the transition from app to app? Can you give me some information?
My boot does not have a home rtos, but my app has an rtos.
Hello,
If the memory spaces are correctly preserved, the RTOS shouldn't interrupt the execution of your program and shouldn't matter if your app or your bootloader is using an RTOS. I will suggest to double-check where are placed the bootloader and the application and be sure the peripherals are you using in the bootloader are correctly de-initialized before entering your application.
Best Regards,
Alexis Andalon